In the Physical
Channel node, select a PHICH channel, then click the
button in the Transmission
Configuration cell to open the PHICH Transmission Configuration dialog
box. Click the Column Preset button
to access a
drop-down
list
that enables you to set the parameters for all PHICH transmissions to
the same value.
Choice: On | Off
Default: Off
Check (On) or clear (Off) to set the channel state.
Range: 0 to 7 (Normal CP) or 0 to 3 (Extended CP)
PHICH Transmission Configuration is showing PHICH Sequence Index in the PHICH group. The relationship between Sequence Index and orthogonal sequence is shown in the table below.
Use the
Data Source
Selection
dialog box to select ,
, or for the selected sequence.